Posted on April 25, 2018 at 15:00Yes, if the project is generated by CubeMx it is not a problem those projects (at least in the latest couple of versions) are generated self-sustaining. But the example projects in the Cube repo are still not. Two di...
Posted on April 25, 2018 at 11:04CubeFW packages uses project files for SW4STM32 (can be read by TrueSTUDIO) using linked resources. As you correctly stated this is to reduce the size of the zip-file.Eclipse/CDT in general does not have a way of imp...
Posted on February 01, 2018 at 12:54Hi atom,When you generated the project for TrueSTUDIO you may have noticed that the default active build configuration 'Debug' uses optimization setting: -Os. This is not good. It means that the GCC compiler is al...