Posted on January 28, 2015 at 05:50<AN3308>9.1 FIFO descriptionThe FIFO buffer is able to store up to 32 acceleration samples of 10 bits for each channel; data are stored in the 16-bit 2’s complement left justified representation.
Posted on November 12, 2013 at 04:51Hello Peter.May be ''Application Note'' AN3308 is help you?CD00290365.pdf: AN3308, 6.3 Free-fall and wake-up interrupts:The LIS3DH interrupts signal can behave as free-fall and wake-up. (and so on...)
Posted on October 23, 2013 at 06:30Hello, Thiago.Sorry, you did not understand me.I would like to say that the values ​​of + /-2g with sensitivity 1mg/LSB not possible to pack in 10bit.Because a 10-bit digit can hold data from 0 to 1023 only.Con...
Posted on October 22, 2013 at 13:18Hello Thiago.How can it's may be, if ''LIS3DH embeds a 32-slot of 10bit data FIFO for each of the three output channels, X, Y and Z.'' and then 4g/1024=~4mg/LSB?Thanks.