Posted on August 17, 2012 at 17:52I gave you the working project. Have you read or compiled it? I did not use an external RAM at that time. In my project do not change anything (except your FATFS realization and a bwa correction in the out_func as m...
Posted on August 14, 2012 at 10:48The only problem is a loss of the PA9 functionality. You don't need to remove R46 - no accident is possible due to the same rail is always present as a main power source.
Posted on August 14, 2012 at 10:48The only problem is a loss of the PA9 functionality. You don't need to remove R46 - no accident is possible due to the same rail is always present as a main power source.
Posted on August 14, 2012 at 10:31You can't allocate 153600 bytes without an external RAM so keep ld script as is. Instead of writing a whole image to the memory buffer try to send it to your LCD by line x MCU height blocks (or, simplier but slowe...
Posted on August 11, 2012 at 13:08Main ijg (libjpeg developer) site:http://www.ijg.org/STM32 firmware:http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32f2-f4_demobuild.zipHave you successed in TJPGD porting yet?Here is a s...