Posted on January 20, 2012 at 20:56Sorry - I'm trying to compile for RAM. Atollic has an option in the new project wizard to build for RAM but the linker script is the same as the build for FLASH. Anyone have an example linker script? Thanks
Posted on January 20, 2012 at 15:23Thanks - three questions then: 1) hideous; I thought I had looked this up and found some magic provision in the 32F4 which allowed writing whilst running? If not - hideous = about 10mS? 2) Flags for relative code ...
Posted on January 20, 2012 at 02:10I'm in the middle of the same thing. I'm using the Atollic toolset for the STM32F discovery board, and now using makefile based development. It would be worth the effort to generate relocatable code if this is p...