Posted on January 13, 2012 at 12:37Weird. Now I'm really confused. The data sheet http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00237391.pdf says that the STM32F205VB has only the OTG HS Controller (see table 2 ...
Posted on January 13, 2012 at 03:26Are you using F205 or F207? The F205 doesn't have the USB OTG FS controller, only the USB OTG HS controller. I'm fairly certain I should be using PB14/15 on the F205, but it would be nice to have some confirmation ...
Posted on January 12, 2012 at 07:22Hi, Can anyone confirm that PB14 and PB15 should be used for DP and DM when using the on-chip full-speed PHY for the STM32F205? The documentation is very unclear about this and I'm concerned that the boards I've ...