Posted on May 17, 2011 at 13:01Hi, I had the same problem last week after having updated the Keil IDE version to the last v3.40.I don't know why , but I had the same error57 message when I entered debug mode , I can only debug in assembly window.The...
Posted on May 17, 2011 at 12:51Dear all, my problem was in the cable that I used to connect PC to STM3210E_EVAL board, now I use a null modem cable and all work fine. Thanks a lot. Stefano
Posted on May 17, 2011 at 12:51Hi, I need help for Bootloader on STM32F103ZET6 device.I'm trying to do the bootloader on the STM3210E_EVAL board with the Flash_loader_demonstrator (v1.1.1) program, in particular I do the following step: 1) I connect...
Posted on May 17, 2011 at 12:51Dear STOne-32, I try with version 1.2 but it doesn't work yet, I have the same error message, does the connection from PC to STM3210E_EVAL is incorrect ? For this I use COM1 port with a non-null cable ( RX and TX not c...