Posted on May 17, 2011 at 12:52Hy Hervett, I using STM32F103RE with ST320F10x-E Eval board, RTC and Timer1 togher without problems: -Timer 1 from HSE 8Mhz-> 48MHz with pwm function at 20KHz frequency -RTC from LSE 32KHz for wakeup during stop mode T...
Posted on May 17, 2011 at 12:52Hy Hervett, I using STM32F103RE with ST320F10x-E Eval board, RTC and Timer1 togher without problems: -Timer 1 from HSE 8Mhz-> 48MHz with pwm function at 20KHz frequency -RTC from LSE 32KHz for wakeup during stop mode T...
Posted on May 17, 2011 at 12:51Hy Stefano, I don't use the bootloader in ST32 micro, but I had use for other micros. The connection from micro to PC is done with a level translator fron RS232 level (+/-12V) to micro level (TTL/3,3V) that provide a l...
Posted on May 17, 2011 at 12:51Hy Wmaguire, I haved use the USB function trying the: -Keil STM32 board and relative example. -IRA stm32 DEMO BOARD and relative example. It's working well and with Hyperterminal: I send and receive fron PC using the l...
Posted on May 17, 2011 at 12:51ehh...... can somebode reset the read out protection???? The read out protection must block the code reading to everybody intrusion!! If it is possible to reset the protection this function is not well working. Please ...