User Activity

Posted on December 21, 2011 at 18:12When I try to enter in suspend mode, as soon as I set it, always receive a wake up interrupt request, and can't do it. I'm not sure if I do the correct process, just set FSUSP and then LP_MODE bit, in USB_CNTR reg...
Posted on December 15, 2011 at 20:30Hello, I'm trying to put USB communication in suspend mode, but when I force wake up, just can read data from PC, but nothing is sent. The interrupt for correct Tx transmition isn't fired. The end point is well co...