Posted on December 19, 2011 at 17:20
Hi
I trying to access UART connection between eval board and pc.
I am using uart 1 on PA9 and PA To change the signals i am using a MAX
From the eval board to the pc the signals are correct, but b...
Posted on December 13, 2011 at 17:31
Hi all
I try to success a connection between PC and SMT32VL-Discovery Board via USART.
The Data receive but are not correct. I tryed everything, but the data i receive onPC are still
wrong.
Ha...
Posted on December 21, 2011 at 08:00Hi Clive1 Thank you for answering. Totally wron means, that i receive only 156 instead of a 'H' which is a 48. I checked the signal with a scope on the input and see its o.k. On the PC side i'm using hyperterminal...
Posted on December 14, 2011 at 16:22Hi clive 1 Thank you for answer. I send 0x53 (hex) and receive 0x25 (hex). I connected the PC over uart (GND, TX and RX without handshake and without flowcontroll). The function setSystemClockTo24() sets:/* HCLK =...