User Activity

Posted on January 09, 2012 at 10:09Hi everybody. I've a remark to do about the ''USBD_GetString(uint8_t *desc, uint8_t *unicode, uint16_t *len)'' function defined in ''usbd_req.c''. When it's called with the function ''USBD_GetString (USBD_PRODUCT_F...
Posted on December 27, 2011 at 17:34Hi everybody. I've just a little question : does anyone knows if the internal temperature sensor of an STM32F107 can be read with ADC2. In the reference manual it's written ''The temperature sensor is internally c...