Posted on February 27, 2012 at 03:00Hi Damien The OV2640 datasheet is available on the web, so are some software and hardware application notes on the OV3640 which is very similar. The explanations on the register settings is the same in some cases ...
Posted on February 13, 2012 at 06:05Hi Renato I have played with trying to double buffer the DMA transfer to SRAM but haven't had any luck. The lack of example code is not at all helpful. I was either going to try and use the JPG compressed mode fro...
Posted on February 13, 2012 at 06:05Hi Renato I have played with trying to double buffer the DMA transfer to SRAM but haven't had any luck. The lack of example code is not at all helpful. I was either going to try and use the JPG compressed mode fro...
Posted on February 07, 2012 at 11:06DamienThe firmware that comes with the evaluation board has a system I think menu option that displays the hardware. On my STM3220g-eval REV B board, the camera is an omnivision OV2640. I think you need to run the...
Posted on February 07, 2012 at 02:31Hi Renato Have a look in the STM32F4 library DCMI examples where you will find an example that uses either the OV9655 or OV2640, the latter sensor is shipped with the STM3220G Rev B board. You need to make a few c...