Posted on May 11, 2017 at 16:30Hello,Concerning the third point, it should be corrected in the last version of STM32CubeMX:The third problem exist not only in V1.15.0, but also in several previous versions. I use FreeRTOS, and I have some interrupts...
Posted on November 23, 2011 at 13:38Hello Eric, Can you try the previous version of STVD: STVD 4.2.1? It seems there is a problem for pathnames with white spaces in version 4.3.0. Robert Jamier ST MCD Tools
Posted on May 17, 2011 at 15:12Hello, The bug only occurs when hardware stepping in some particular cases. If you execute the program without hardware stepping, it works. There are two possible workarounds if you want to step: - use software steppin...
Posted on May 17, 2011 at 15:12Hello, More generally, differences between two labels in two segments don't work if the segment start addresses are defined in another file. To avoid this, compute differences within the same segment and use constants ...