Posted on May 04, 2011 at 21:30Hi Fabio, See my comments above. In your file list you are missing a discover.elf file; also I suspect you are missing a few more library modules. Once you have all the object files set up you need to compile each modu...
Posted on April 30, 2011 at 03:18I am now building and debugging successfully but I went to create a makefile for the project (Project->Export Makefile) and I get the same error. Is there a workaround for this as well?
Posted on April 29, 2011 at 05:17I can confirm I have achieved a successful build using the steps outlined by Phil, with some additions.There are a number of comments I would make The .o files need to be empty; my first attempt was to simply copy...
Posted on April 24, 2011 at 00:39I am also seeing this problem. STVD 4.2.1 patch 1 running on Vista 32-bit.I have installed both Cosmic 32K and Raisonance compilers and I get the error with both. I am using the example workspaces from the Discover p...