Posted on October 10, 2017 at 18:26Hi,I am using a stm32f411 with 512Kbyte flash.I want to create a dump hex file of the flash as a backup.What is the Value of 'Size' 0x???? I have to write into the st link utility form to create an exact dump of 5...
Posted on September 08, 2014 at 13:25Hi, I want to use the STM32F4 Discovery as a data logger. Is there a working composite USB example project out there? (I'm using eclipse + FreeRTOS, but Keil works for me too). BR Emilio
Posted on April 09, 2014 at 23:52Hi, I generated a project with an lqfp100 STM32F427VIT6 and I had following setup: - FreeRTOS - USB CDC FS - FatFS / SD Card - Keil MDK-ARM 4.74 - no DMA - freertos default settings The generated Project is building ...
Posted on June 13, 2013 at 03:19Hi Guys, the last times I had so many technichal questions and I'm glad that it ended in a good way. My Project is finshed now and I would like to share the results with you and the sucess story with choosing STM32F4...
Posted on June 10, 2013 at 17:57Hi, is it possible to use this two or three Devices on the FSMC or what is the max of possbile peripherials on the FSMC bus? I wanted to connect my Display and an external SRAM (like the one of the STM32 Eval Board) w...
Posted on March 03, 2015 at 22:49Problem is easy to solve... take a look on your HAL Interrupt Handler for the U(S)ART. It is totally overloaded. Just clear everything out and keep a code that moves the usart received data to ur buffer and clear the...
Posted on September 08, 2014 at 13:39Hi, I want to use the STM32 F4 Discovery as a composite device too. Did you made some progress? Is it possible to get the Project? Best regards, Emilio
Posted on July 02, 2013 at 23:26Hi, for 41$ there is also a full featured raspberry PI board or Beagleboard with 256MB/512MB Ram. I don't understand where the benefit is. Because the other Boards with Cortex-Axx are more powerful and they have full ...
Posted on June 13, 2013 at 21:08The Kalman-Filter is using 2x 3D Accel + 2x 3D Gyro + 2x Mag but the Mag is just for the secular Information-Fusion (simplified without going to deep into the algorithm: ''Hey I'm sensing your motion and it's might ...