Posted on October 06, 2016 at 16:01 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on November 08, 2016 at 12:29A quick follow-up to this problem: The limitation was confirmed by ST and should get published in the errata sheet.
Posted on October 11, 2016 at 15:54
OK, reporting back...
I got one F469I Discovery board and tested the same code as shown above...
Ignoring the fact that the SDRAM on the discovery board is of another type (32 bit and 4 banks),...
Posted on October 07, 2016 at 12:15Hi! Thanks for the hint. I already ordered the discovery board and will report back if the same problem occurs there.
Posted on October 06, 2016 at 22:10Unfortunately, this is not possible in this design because the STM32 in question is in a BGA package and the other alternate pins are not accessible because they are not fanned out. :(
Posted on July 26, 2013 at 14:02Hello, I am in the process of developing a USB enabled monitoring device using a STM32F103 microcontroller with native USB support. Since the company I am working for does not own a USB Vendor ID and the number of uni...