User Activity

Posted on March 22, 2012 at 02:32Hi I have several different motors that I would like to drive (one at a time) using the same hardware and firmware based on the STM32 FOC PMSM libraries. The motor selection is indicated to the processor with a DIP s...
Posted on February 15, 2012 at 01:24Hi, I'm working with the PMSM firmware library V3.0 to make a motor control using the STM32F103C8T6 processor operating on my own board. I am working with the provided non-RTOS project which was originally configu...