Posted on March 04, 2013 at 15:21The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on March 04, 2013 at 20:02Like I said its code that worked on the F103 MCU I only have a F demo board, never got the L series, just had some prototypes of our PCB made with a L151 Low power MCU to see if I could get the Run time Power down. I...
Posted on May 17, 2011 at 14:25 Thanks, yes the standby was a result of the complete project, I do not need to wake up every second in standy but I used that interrupt to check if the RTC was running, kept the main in an endless loop now, and I get ...