Posted on May 17, 2011 at 13:54Thanks for your response. I also decided to make provision for both situations by placing 0Ohms's. One reason I read in the docs where one would need to connect to CRS_DV line rather than the RX_DV line is if you need ...
Posted on May 17, 2011 at 13:54I have the same question at the moment, so I am bumping this post. I am not sure where CRS_DV on the PHY should be connected to. It is connected to PA0 on the eval kit, which is according to my understanding only used...