Posted on May 17, 2011 at 14:18We have those pins : ADC123_IN0 to ADC123_IN3 : 4 pins ADC12_IN4 to ADC12_IN9 : 6 pins ADC3_IN4 to ADC3_IN8 : 5 pins ADC123_IN10 to ADC123_IN13 : 4 pins ADC12_IN14 to ADC12_IN15 : 2 pins ========= Total 21 pins There a...
Posted on May 17, 2011 at 14:18That's ok if you don't need all the ADC channels available on the MCU. If you need all the channels you have a problem because there are less ADC input pins that the number of ADC channels. Or is there something trivia...
Posted on May 17, 2011 at 14:18Hi bulmer.g I understand that the pins are multiplexed on the MCU, but how to you connect your 2 or 3 (depending on the pin) analog signals coming from the real world to a single MCU pin ? That's what I don't figure ou...