Posted on May 17, 2011 at 14:15''Unless the Flash has specific areas that are less-susceptible to errors, if any bit can be damaged in the flash, it is equally likely to be at any location - so it is equally likely to be within the CRC verification ...
Posted on May 17, 2011 at 14:15Flash verification is one of several tests used to conform to the IEC60730 safety standard, e.g. for a washing machine controller. Your points are valid, but say that one bit of the flash has been altered, e.g. due to ...