Posted on May 17, 2011 at 14:11Okey, i guess that ''USB JTAG debug pod'' is a product to connect the board to the computer, is it possible to buy it on http://www.st.com/, cause i can't find it if anyone would like to give me a link it would be appr...
Posted on May 17, 2011 at 14:11i found this IAR Embedded Workbench for ARM, v. 5.50, Evaluation version which i will download when i got the time. And cross-compile it to .bin. But when i have done that i need to get it into the flash, is it possi...
Posted on May 17, 2011 at 14:11The program is written in a freeware C++ compiler, don't have the name with me... I am using an USB cable from the PC to the board USB-B port... I can without problem use the card as a USB memory but i have no idea how...