Posted on May 17, 2011 at 13:58Thanks I was able to see what was in the flash memory with J-MEM....J-Flash can't detect my flash on my iNemo board!! Maybe normal since the is no physical flash on the board and there is 512Kbytes in the STM32F103REST...
Posted on May 17, 2011 at 13:58I just look at the schematic and the USART1 on iNemo is not used!!! Only USART2 is used to communicate to the expansion serial connector!! Is it possible to download a bootloader :tiny_kernel_bootloader that uses the ...
Posted on May 17, 2011 at 13:58I forgot to say that i'm trying to use uClinux on an iNemo board! Same processor but different componement!! Still has one UART port but on the plans the say it UART2?? weird!! thanks
Posted on May 17, 2011 at 13:58I have many question about what you just told me 1. The jtag-J-Flash can't seem to see my flash on the iNemo board is that normal?? 2. In order to run the uClinux on the boat do a really need to change the boot loader?...
Posted on May 17, 2011 at 13:58Hi i have the same problem!! i'm trying to figure it out right now! Sorry i don't have a direct response to that!! but have you tried out this prog http://www.er-forum.de/obd-diag-dl/index.php?action=downloadfile&filen...