User Activity

Posted on April 19, 2013 at 10:50 Hello, I've doubts regarding the access of an external SRAM (IS61WV102416BLL) connected to the FSMC bus that has the following spe cifications . This SRAM is organized as 1024K x 16-bit . ...
Posted on March 26, 2013 at 12:02Dear all, I have developed a board on which a STM32F205 microcontroller is connected to an asynchronous external SRAM (ISSI IS61WV102416BLL) which has read/write access times of 10ns. This RAM is used as a picture b...
Posted on January 16, 2012 at 11:25Hello, I plan to use a STM32F207 MCU in order to display pictures stored in a SD card on a controller-less 7 inches TFT display (WVGA, 800x480, 18bpp). The pictures are static. Is it possible to interface such a di...
Posted on May 25, 2010 at 11:01USB OTG with two connectors (STM32F105)