Hello,As of today STM32 support SPR and has to be used with TCPP0x.Our next version TCPPE with an update software for STM32 will be compliant with 140 W (EPR) but it is not available today.Regards
Hello, The current products (TCPP0x + STM32) are able to manage up to 100 W (SPR mode). The next solution (TCPPEx + STM32) will be able to manage up to 240 W (EPR mode). In your case the suitable product will be TCPPE2.Regards.Philippe
Dear Gorkem,You are right this is quite new and I am not aware of any IC able to manage 240 W EPR either with µC or stand alone. We are working on it but we wont have product before Q3-2024 as the product is today not fully defined.CC...
Dear Gorkem,Protection is like insurance. Everybody does not want to pay for that because it is useless until you get a crash. In our case the crash is either a surge or a short circuit to Vbus. So it is better to add protection.When do you...
Dear Gorkem,Thanks for the detailed description.TCPP0x series has been developed several years ago when Power Delivery was 100 W maximum. So the limitation of the TCPP0x series is 100 W because of the voltage of the technology used. For th...