Posted on May 17, 2011 at 13:50Hi Chikos, AN2557 contain IAP example, it has two images inside - the first one is the boot loader and the second one is an example that turn the LEDs on/off. both images works OK whenever using debugger only the jump ...
Posted on May 17, 2011 at 13:50Hi Giannetti, thanks for you reply. I got Hardware Error when ever it jump. I'm using the exact example of AN2557, i didn't change a thing. it met the code and get to the jump instructions. I also change the IAR worksp...