Hi Mike,if not done yet, I suggest you to start with this example which is included in x-cube-azrtos-f4->https://github.com/STMicroelectronics/x-cube-azrtos-f4/tree/main/Projects/STM32F429ZI-Nucleo/Applications/NetXDuo/Nx_TCP_Echo_Server
Hi, you can refer to the below UMhttps://www.st.com/resource/en/user_manual/um2642-description-of-stm32wl-hal-and-lowlayer-drivers-stmicroelectronics.pdfthanks and Regards
Hello, can you please let us know which Nucleo or Discovery board you are targeting?Normally in our Nx_TCP_Echo_Server examples UART is set by default as follows:BaudRate = 115200 baudWord Length = 8 BitsStop Bit = 1Parity = NoneFlow control = NoneCa...
Just to add a clarification, system memory bootloader address is mentioned on AN2606 and for STM32H7 it always differs from system memory base address. On STM32H72/3/4/5 bootloader address is 0x1FF09800 while for STM32H7A/B it is 0x1FF0A000.