Posted on May 17, 2011 at 13:45For what is worth, in the end the problem was with a (apparently) stripped down version of stm10x*_uart.h... Apparently my predecessor must have gotten and modified this. I replaced it with the one from the ST USART ex...
Posted on May 17, 2011 at 13:45SUCCESS! This morning I downloaded the ST example on USART and after changing the ICF (for my target hardware) it compiled and .....Printf Example: retarget the C library printf function to the USARTUSART1> I got that ...
Posted on May 17, 2011 at 13:45I spent some hours on this issue last night and I can't make any progress. All I can think is that perhaps there are some issue with the IAR initialization. I guess unless anyone else has any suggestions or complete US...