Posted on May 17, 2011 at 13:43These problems has been solved. If you use Code example for STM3210C,B,E evual to program MCBSTM32, chose STM3210C-eval board on Keil (scrolling menu at the right of Load button). It works because STM3210B has a Medium...
Posted on May 17, 2011 at 13:43Hi, I used Flash Loader to flash stmdfu.hex. No problem to download it on the board (MCBSTM32) but the board is not recognized as an DFU Device. So I've got the same problem after programming DFU example with Jtag (STM...
Posted on May 17, 2011 at 13:43Thx, Now, my problem is : - I installed, compiled and download STM32_USB-FS-Device_Lib_V3.1.0/Project/Device_Firmware_Upgrade from UM0424 but my computer doesn't recognize the board (MCBSTM32). - I select STDFU.inf an...
Posted on May 17, 2011 at 13:43Hi, Little question that could help me much. To use Flash Loader can't I use USB connector ? Am I obligated to use Com ? Thx
Posted on May 17, 2011 at 13:43Hi, I've download STM32_USB-FS-Device_Lib_V3.1.0. I change clock parameters, compiled the project and downloaded it into Keil MCBSTM32's µC. Of course, my device is ''Unknowed'' but the Flash loader doesn't recognize ...