Posted on May 17, 2011 at 10:00Hi Hans, If you are using the M25P64 (or same family) then you can use 'ssp_flash_driver.c' (from this site) to drive the IC. It has all the useful functions you need. From a hardware point of view, the flash IC can be...
Posted on May 17, 2011 at 10:00Hi, If someone can solve my problem ''STR9 Timer Prescaler'' posted on this board, I will upload the full IAR project I did for Mass Storage with M25P64 (works on STR910-EVAL board). Regards.
Posted on May 17, 2011 at 10:00Hi, If someone can solve my problem ''STR9 Timer Prescaler'', I will upload the full IAR project I did for Mass Storage with M25P64 (works on STR910-EVAL board). Regards.