Posted on August 19, 2008 at 07:28Hi Luca, Thanks for the reply. I think this is the linker file (.lkf): # LINK COMMAND FILE AUTOMATICALLY GENERATED BY STVD7 # SHOULD NOT BE MANUALLY MODIFIED # # Put you segment configuration here # define the .shar...
Posted on August 15, 2008 at 12:54micro: ST7FLITE39 c compiler: cosmic 16k 4.5.7 IDE: ST Visual Developer 4.0.1 Hi, I'm setting up an interrupt routine to populate an array, and then calculate the sum of the elements of the array as part of an RMS a...