Posted on May 17, 2011 at 13:35Hi jj.sprague It's working! finally :) I was testing all things i could think off, and then i saw the TFT display on the eval board flickering. It seems that FSMC pins are also connected to the TFT. The OE, WE and all ...
Posted on May 17, 2011 at 13:35Hi, sorry if i wasn't clear enough. When i mention the SRAM in my post i refer to the external SRAM IC on the STM3210E-EVAL board. The Keil IDE can indeed read the memory and display it when the program is running. Quo...
Posted on May 17, 2011 at 13:35Hi, I am using a STM3210E-EVAL board in combination with Keil and an Ulink2. I am trying to use the FSMC in combination with the SRAM on the board. I studied the SRAM example program from STM. Works perfect. I will be ...