Posted on May 17, 2011 at 13:28Looking at the Docs it appears the STM32C can but used as USB host so is there example software so the STM32C can connect to a USB flash drive? If so how much code/ram space does it take? What file systems does it sup...
Posted on May 17, 2011 at 13:28For the TeaClipper solution most times we send the clipper to the customer and have them update all of the units then send the clipper back to us. We have been buying the clippers from Mouser http://www.mouser.com/Sear...
Posted on May 17, 2011 at 13:28We are looking for a solution that does NOT need a PC to do the update. (your suggestion did seem like a good solution if using a PC was a choice). The users most times do not have a PC so I am looking for a low cost s...
Posted on May 17, 2011 at 13:28Yes I have read the AN2606 and have run the Flash loader demonstration. The issue with this approach is the need to use the Uart1 interface. In many of our products the Uart pins would be tied to other devices so I wil...
Posted on May 17, 2011 at 13:27We are switching to STM32 processors and are looking for a simple way to update units out in the field. In the past we used Pics (dip package in a socket) and would just send a new chip for the user to put in the socke...