Posted on May 17, 2011 at 09:59If you have Flash bank 1 configured as the boot bank and never change the mapping of the Flash banks so the exception handlers are always executed from bank 1, you need to have some sort of flag, say in a particular RA...
Posted on May 17, 2011 at 09:59I am looking for a way to programmatically determine the product ID and revision level of the CPU die on an STR91x part. I am able to read 0x9120 from the OTP memory but I need a list to interpret what this number mean...
Posted on May 17, 2011 at 09:47Hello ly_liuyang_ly From what I read in the ST application note AN2633, there should be 3 ''dummy'' instructions after executing the command to enter a low power mode if the system is running from the 32 kHz clock as y...