Posted on May 17, 2011 at 13:27Thanks for answering. Yes it's an external ADC with a max sampling speed of 40Msps. The problem i guess is it wants a clocksignal with 45-55% duty cycle to function properly. Could I generate such a clocksignal at 8MHz...
Posted on May 17, 2011 at 13:27Hi, I'm thinking of trying STM32 for a simple DSO-project. What would be the max speed for reading 12 pins (external parallel ADC) and transfer it to SRAM using DMA? After reading the datasheet I guess somewhere around...