Posted on May 17, 2011 at 13:23I have the same problem... Did you find a solution yet ? The CAN1 interface is working OKe (send & receive) The CAN2 interface is ONLY sending, NO receive possible. Also when I use both interfaces (send from CAN2 to CA...
Posted on May 17, 2011 at 13:17I cannot get the VCOM working (using my own hardware). Using KEIL compiler and a SMT32F105RC. Has anyone made a KEIL version of the given RC1 sample (VCOM part). The computer (Vista & XP) is not detecting a correct dev...