Posted on May 17, 2011 at 13:26Thank you for you replying! Yes I use interrupts in the code I try it in the flash memory in the same way and it success I mean I setup the start address of the Flash as 0x08000000, and set interrupt vector: NVIC_SetVe...
Posted on May 17, 2011 at 13:26Hi all, We can excute code in RAM with JTAG, and debug it we only need to do flowing steps 1> Setup IROM1 start address: 0x20000000 size:0x3000 IRAM1 start address: 0x20003000 size:0x1000 2> Load Ram.ini file while de...