Posted on May 17, 2011 at 15:04Oh thanks for your attention ^^ Follow your link, using STVP, i just simple configure the wait stage to ''1 wait stage'' in the option byte tab, and it runs at 20MHz clock ^^ Many thanks ^^
Posted on May 17, 2011 at 15:04Hi. I'm using STM8S207K6, it's ok with 16MHz crystal or lower. But with 20MHz crystal, it works only when i set the prescale = 2; (CPU clock = 20MHz/2 = 10MHz). So what should i do to make it work with 20MHz CPU-clock?...
Posted on May 17, 2011 at 15:03Thanks Luca. So i think that in STVD,there is no function or library to be build-in. All the operation must be made by ourself. However, it's OK ^^ Thanks for your help ^^
Posted on May 17, 2011 at 15:03Thank you, Mozra27 ^^ I already get all documents on that link, but still can not find any instruction about C language. For example, i want to know in STVD, an integer variant is 2bytes or 4bytes... and some function ...
Posted on May 17, 2011 at 15:03Hi, i'm newbie ^^ I'm using STVD, through ''help'' menu, i can't find any C instruction, function... I'm looking for C instructions, functions, variant definition... can any body help me. Thanks.