hassan_mj
Associate II
since
2018-07-19
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About hassan_mj
Options
Report User
User Activity
Posts
Replies
JTAG and SPI1
2009-12-15
Posted on December 16, 2009 at 02:19JTAG and SPI1
STM3210B with IAR compiler
2009-11-24
Posted on November 25, 2009 at 08:40STM3210B with IAR compiler
Re: JTAG and SPI1
2011-05-17
Posted on May 17, 2011 at 13:34I have to use SPI1 port which is shared with JTAG. Will I be able to debug my firmware while I am using the SPI port, or this is not allowed and the JTAG will be confused. Thanks
Re: STM3210B with IAR compiler
2011-05-17
Posted on May 17, 2011 at 13:31Hi, Is there any project for IAR with the STM3210B development kit? Regards, Hassan