Posted on May 17, 2011 at 13:31I'am sure that the hardware is correct, because if I configure the pins in Open Drain, I can move them. I use the STM32F101RBT6 Do you use a STM32101 or other?
Posted on May 17, 2011 at 13:31Help I use the I2C2 with pin PB10 and PB11, but when I use the command I2C_GenerateSTART(ENABLE) only the pin PB10 goes low and so I can't generate the Start Condiction. Can you help me?