Posted on May 17, 2011 at 13:18''Variable'' signal this is what I mean, thx. ^^ @M3allem: I have read the application note, but I can't find anything wrong. As I wrote, I use the KickStart Kit and connected a frequenz generator directly to the Pin. ...
Posted on May 17, 2011 at 13:18Hello, I have a problem with the ADC, if I read static values everything is fine, but dynamic values are wrong. parameter: µC: STM32F103RBT6 IAR KickStart Kit VDDA: 3,3 V VSSA: 0 V samplerate: 25,6 kHz signal: 1 V pea...