Posted on May 17, 2011 at 13:37We have set readout protection in a computer, and now we want to reprogram it via SW. Even though we have set the Cortex target driver setup to Erase Full Chip, it will no longer allow us to write to the computer eithe...
Posted on May 17, 2011 at 13:22I get the same thing. IWDGRST doesn't work with SWD which makes it very hard to program behavior after a watchdog reset. Also, NVIC reset doesn't work while debugging. If either of these behaviors is a settable option,...
Posted on May 17, 2011 at 13:15Yes we have also noticed some movement in the first 32 bits. If those were the top of the count, they wouldn't move or would move randomly and I'm not seeing that. So I'm still guessing they are something else. There i...
Posted on May 17, 2011 at 13:15We need to find a solution and adding a serial number chip when we already have a serial number seems a waste. I've started breaking down the numbers. If others are willing to help, we might be able to decode enough of...