Posted on January 18, 2010 at 03:20 We have been using AN971 I2c_eepr.asm code on a ST72F One of our I2C peripherals has changed from having an 8 bit sub_add to having 16 bit. Would you make suggestions on how to modify I2c_eepr.asm to work with a...
Posted on July 30, 2009 at 06:18I need to be able to power up a peripheral on PA3 at 3.0V and 15mA when Vdd of the F264 is 3.0V. Is that doable? PA3 will typically be low, but when it goes high can it provide the 15mA without sagging it's output bel...