Posted on May 17, 2011 at 15:03According to documentation when SWIM mode is enabled (register CFG_GCR, SWD=0), the SWIM pin can not be used as general purpose I/O. I should have disabled SWIM mode earlier (SWD=1).I suppose that the microkontroler is...
Posted on May 17, 2011 at 15:03Hi Ok so I should replace the microcontroller? According to documentation it's possible or I understood incorrectly. SWIM disable By default, after an MCU reset, the SWIM pin is configured to allow communication with a...
Posted on May 17, 2011 at 15:03Hi, I have a problem with communication board (STM8S/128-EVAL/A), I use in my application port_H as output but then I change for the port_D. I compiled and programmed but during verify was error. Now I haven't communic...