Posted on May 17, 2011 at 15:03Hi there, I am having difficulties in implementing a PWM for one output in TIM1 and making a time base generation in TIM2. (STM8S105K6) Regarding the TIM2: I want to have an internal 1920Hz signal without using the out...
Posted on May 17, 2011 at 15:02Hi mozra, Thank you very much! :-] Only one more thing regarding the comment: ''The ADC1 scan mode works for all the channels available on the product'' The datasheet says: ''Scan mode for single and continuous convers...
Posted on May 17, 2011 at 15:02Hi, I would like to know how to use the ADC1 DATA BUFFER in order to acquire 5 channels simultaneously. I use the STVD 4.1.1 with Cosmic compiler and the FW library. Is the code bellow correct? (The ADC1Init is used fi...