Posted on May 17, 2011 at 13:31Thanks ST1, but I don't want to map it as RS232 COM, rather I'd like to use ftd2xx library in my project. One of the reasons for that is because I'd like to control the STM32's bootmode pins from the FTDI. Other reason...
Posted on May 17, 2011 at 13:31Hi, I need to make a GUI application to load the FW to STM32. I was thinking to use STBLLIB, but it seems to be impossible as the UART is hardcoded inside. The idea is to use any custom USB to UART converter(like FTDI)...
Posted on May 17, 2011 at 12:46Hi, I tried http://www.emedt.com/armdt/ with Wiggler type JTAG for debug. I was able to connect the target and read memory only. Unfortunatelly I was not able to debug code or view registers. I don't know what is the r...