Posted on May 17, 2011 at 12:37The reasons are simple: 1.Programming the flash memory. 2.Your PC doesn't have drivers. 3.If you are using the Demo version from st then it was working properly. 4.Check the BOOT options, power supply to the board and ...
Posted on May 17, 2011 at 12:36Like USART1 and USART2 , we can see the printf statements in hyperterminal.so for USART3 what we have to do? to see the ''STATEMENTS'' Mr.ST7 :-]
Posted on May 17, 2011 at 12:36Hi, Can anybody tell me how to use the USART3 for printf function and I want to see the statements in Hyperterminal. :-Y
Posted on May 17, 2011 at 12:36Hi Techies, STM32BT-EXT-EVAL Evaluation Board is designed as daughter board which can be connected to STM3210B or STM32B10E evaluation board and we can connect STM32 performance stick. The ST's Bluetooth module SPBT25...