Posted on May 17, 2011 at 09:58Hello, I'm using a STR912FAW44, and I'm trying to set the DISEST bit in the MC_PCR1 register, to disable emergency stop of the PWM, since I'm just using the PWM to trigger ADC conversions. However, I cannot get the DIS...
Posted on May 17, 2011 at 09:58I'm running the A/D converter in scan mode, with 7 channels enabled. Conversion mode is single. I'm using a STR912FAW44. PCLK is 48 Mhz. I field the interrupt, clear the flag, read the conversions, then start the next ...
Posted on May 17, 2011 at 09:58Hi Lakata, Thanks for the feedback. I took a look at 91x_map.h, but mine doesn't have the DDR and CR2 fields - my last field is the PRS. I am not using the DMA on the ADC, so I guess that's why I haven't noticed before...