Posted on May 17, 2011 at 09:57Hello eris, I have connected NSS slave pin to GND and the slave receive data correctly. And it is a must to connect NSS master pin to VCC if I want to transmit data of the slave to the master? I'm working with a board ...
Posted on May 17, 2011 at 09:57Hello, First of all, sorry because my English is quite bad. I need to comunicate two STR910 micro via SPI. I've chosen SSP1 port for the communication. One of the micros will be the master, and other will be the slave....