Posted on May 17, 2011 at 13:29Hi! Now I get a .bin file out of the linker - there was an option ''Output Converter''. But it does not start - the memory is filled with the same info as I program it with JTAG...
Posted on May 17, 2011 at 13:29Hi! Thanks for your answer. I get a .out format out of the IAR Embedded workbechn, but someone told me just to change it to .hex in the Linker Options. Is this correct? I looked the memory up with JTAG - the file conta...
Posted on May 17, 2011 at 13:29Hi! I've written a program with IAR Embedded Workbench, compiled it, linked it and with JTAG it works fine. Now I wanted to send it via bootloading - but it does not work. The flash loader demonstrator sais, that the b...