Posted on May 17, 2011 at 10:14Hello, I am unable to build the PMSM and ACIM examples included with the kit without making any modification. That's not completely true. If I build them once, no errors are reported. If I build them a second time, (ju...
Posted on May 17, 2011 at 10:14I think I solved the problem for the ACIM example. Turns out that one of the grayed out options under projects/options/linker is to start at ''__iar_program_start''. So, if I add the following line to stm32f10x_vector....